AXIS#.WS.NUMLOOPS
Description
This parameter sets the maximum number of wake and shake repetitions. AXIS#.MOTOR.PHASE is calculated as mean value of all wake and shake repetitions.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
counts |
|
Range |
0 to 20 counts |
|
Default Value |
5 counts |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.WS.NUMLOOPS | 0x5013 | 0x2 | USINT | - | - | RW | False |
| AXIS2.WS.NUMLOOPS | 0x5113 | 0x2 | USINT | - | - | RW | False |